NPC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
3,246 次查看
zhhq123
Contributor II

Hi,
I want to Use MSEO1 as SPI_SI, EVTO as SPI_SO and MSEO0 as SPI_SCLK,Is there any Example code or advice ?
Best Regards.

0 项奖励
回复
1 解答
3,214 次查看
zhhq123
Contributor II

I misunderstood the use of these PINs.

I used SIU to cofig these PINs to work as GPIO.

I used GPIO to stimulate SPI.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,220 次查看
juama
Contributor I

Also let me know when you found, the solution for that!

thanks

0 项奖励
回复
3,215 次查看
zhhq123
Contributor II

I misunderstood the use of these PINs.

I used SIU to cofig these PINs to work as GPIO.

I used GPIO to stimulate SPI.

0 项奖励
回复
3,234 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's good to mention which device you use...

Regards,

Lukas

 

0 项奖励
回复
3,222 次查看
zhhq123
Contributor II

MPC5634

0 项奖励
回复