NO CAN Communication in NXP DEVKITCOMM BOARD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NO CAN Communication in NXP DEVKITCOMM BOARD

1,030 次查看
SAchary11
Contributor I

Actually I have 2 questions related to the NXP DEVKIT- MPC5748G and NXP DEVKIT- COMM Board

 

1) I have observed that when there is a USB/UART connector, I see that proper communication in the CAN A, CAN B and CANC of the Devkit COMM(I mean all the channels), if I change the jumper and use only external power supply CAN channels are not acknowledging to the frame sent from the other ECU

I have changed the Jumper to the external 12V supply as per the Schematic.

Can anyone tell what could be the reason for it? 

 

 

0 项奖励
回复
1 回复

1,021 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to check supply pins on COMM board. If VDD and P5V0 are correct then there should not be issue I think.

BR, Petr

0 项奖励
回复