NO CAN Communication in NXP DEVKITCOMM BOARD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NO CAN Communication in NXP DEVKITCOMM BOARD

1,029 Views
SAchary11
Contributor I

Actually I have 2 questions related to the NXP DEVKIT- MPC5748G and NXP DEVKIT- COMM Board

 

1) I have observed that when there is a USB/UART connector, I see that proper communication in the CAN A, CAN B and CANC of the Devkit COMM(I mean all the channels), if I change the jumper and use only external power supply CAN channels are not acknowledging to the frame sent from the other ECU

I have changed the Jumper to the external 12V supply as per the Schematic.

Can anyone tell what could be the reason for it? 

 

 

0 Kudos
Reply
1 Reply

1,020 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to check supply pins on COMM board. If VDD and P5V0 are correct then there should not be issue I think.

BR, Petr

0 Kudos
Reply