Multiple CAN FRAME IN Single Sample Time MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple CAN FRAME IN Single Sample Time MPC5744P

1,089件の閲覧回数
AdhamGad1
Contributor I

when i set a single signal to be sent two times with different values in the sample time.

The second always overwrites the first value..Can you please provide a solution?

0 件の賞賛
返信
1 返信

1,073件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could you please describe a case in more details?
Does it mean you have single Message Buffer (MB) defined for reception and if 2 messages are sent from other node, first message in the MB is overwritten?
It could happen if the MB is the matching one and is free-to-receive. 
Read Receive and Matching process chapters of the device RM.

BR, Petr

0 件の賞賛
返信