Microcontroller which supports Flexray,CAN and ADAS development?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Microcontroller which supports Flexray,CAN and ADAS development?

5,162 Views
raghavendrap
Contributor I

Dear All,

 

Which microcontroller and the evaluation board should i purchase for the automotive communication protocals like Flexray,CAN and LIN development.

 

Also does freescale has any boards targeting advanced driver assistance functions (ADAS)?

 

Thanks and Best Regards,

Raghavendra P

Labels (1)
0 Kudos
Reply
4 Replies

4,443 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I recommend you microcontrollers from 57xx family. There are few possibilities, which meet your requirements about Flexray, CAN and LIN.

Please look at the following microcontrollers:

MPC574xB/C/D/G|32-bit MCU|Gateway|NXP 

MPC577xK|32-bit MCU|ADAS|NXP 

MPC5777M|32-bit MCU|Powertrain|NXP 

About ADAS module, there are two main devices:

MPC577xK|32-bit MCU|ADAS|NXP 

S32R Radar Microcontroller|NXP 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 Kudos
Reply

4,443 Views
raghavendrap
Contributor I

Hello Martin,

Thanks for the information.

1.Can we use configuration tool like the Rappid Tool for startup code and low level driver code generation?

2. Any IDE like the S32 Design Studio support the MP57xx series?

3. Do we have a evaluation boards for the above micro's?

Regards,

Raghavendra P

0 Kudos
Reply

4,443 Views
martin_kovar
NXP Employee
NXP Employee

Hello Raghavendra,

1) Yes, RappiD Init could be used for startup code, but I am not sure about low level drivers code generation. I will ask my colleague on Monday.

2) Green Hills and also WindRiver has their own solutions, but both are under license. Please look following links:

Real-Time Operating Systems (RTOS), Embedded Development Tools, OptimizingCompilers, IDE tools, Debu... 

Wind River 

3) Here is link for MPC5777M EVB and MPC5748G EVB

MPC5777M Evaluation Board (EVB) and Adapters|NXP 

Evaluation System for MPC574xB/C/G Family|NXP 

About MPC5775K and s32r please contact you local distributor. He will provide you more accurate information.

Distributor Network|NXP 

Regards,

Martin

0 Kudos
Reply

4,444 Views
raghavendrap
Contributor I

Hello Martin,

Thanks for the information

Is Autosar_CS software a free package for Evaluation System for MPC574xB/C/G Family|NXP ?

Do we have a Codewarrior Environment with GCC compiler for above micro's?

0 Kudos
Reply