Microcontroller which supports Flexray,CAN and ADAS development?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Microcontroller which supports Flexray,CAN and ADAS development?

5,051件の閲覧回数
raghavendrap
Contributor I

Dear All,

 

Which microcontroller and the evaluation board should i purchase for the automotive communication protocals like Flexray,CAN and LIN development.

 

Also does freescale has any boards targeting advanced driver assistance functions (ADAS)?

 

Thanks and Best Regards,

Raghavendra P

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

4,332件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I recommend you microcontrollers from 57xx family. There are few possibilities, which meet your requirements about Flexray, CAN and LIN.

Please look at the following microcontrollers:

MPC574xB/C/D/G|32-bit MCU|Gateway|NXP 

MPC577xK|32-bit MCU|ADAS|NXP 

MPC5777M|32-bit MCU|Powertrain|NXP 

About ADAS module, there are two main devices:

MPC577xK|32-bit MCU|ADAS|NXP 

S32R Radar Microcontroller|NXP 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 件の賞賛
返信

4,332件の閲覧回数
raghavendrap
Contributor I

Hello Martin,

Thanks for the information.

1.Can we use configuration tool like the Rappid Tool for startup code and low level driver code generation?

2. Any IDE like the S32 Design Studio support the MP57xx series?

3. Do we have a evaluation boards for the above micro's?

Regards,

Raghavendra P

0 件の賞賛
返信

4,332件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Raghavendra,

1) Yes, RappiD Init could be used for startup code, but I am not sure about low level drivers code generation. I will ask my colleague on Monday.

2) Green Hills and also WindRiver has their own solutions, but both are under license. Please look following links:

Real-Time Operating Systems (RTOS), Embedded Development Tools, OptimizingCompilers, IDE tools, Debu... 

Wind River 

3) Here is link for MPC5777M EVB and MPC5748G EVB

MPC5777M Evaluation Board (EVB) and Adapters|NXP 

Evaluation System for MPC574xB/C/G Family|NXP 

About MPC5775K and s32r please contact you local distributor. He will provide you more accurate information.

Distributor Network|NXP 

Regards,

Martin

0 件の賞賛
返信

4,333件の閲覧回数
raghavendrap
Contributor I

Hello Martin,

Thanks for the information

Is Autosar_CS software a free package for Evaluation System for MPC574xB/C/G Family|NXP ?

Do we have a Codewarrior Environment with GCC compiler for above micro's?

0 件の賞賛
返信