MPC5xxx: MC_ME RUN_PC and LP_PC Configuration Registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5xxx: MC_ME RUN_PC and LP_PC Configuration Registers

跳至解决方案
3,851 次查看
cholland
Contributor V

Hi,

Specifically for the MPC5746C

I am having some issues with setting the RUN_PC and LP_PC Configuration Registers.

I am trying to use PC7 and LP7 configurations for LIN1. When I try to enter initialization, it fails with "Error : Error in ONCE status register during instruction execution."

I know the problem is with RUN_PC[0]. If the modes for PC0 are enabled, then it works fine, but I should be setting the PC7 and LP7 for LIN1. I don't understand what the problem is.

Thank you,

 

MC_ME Registers.png

 

 

0 项奖励
回复
1 解答
3,811 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it looks like it is caused by DBG_F bit in PCTL51 register. If you configure this bit as '0', is it working?

Regards,

Lukas

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,812 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it looks like it is caused by DBG_F bit in PCTL51 register. If you configure this bit as '0', is it working?

Regards,

Lukas

 

0 项奖励
回复
3,794 次查看
cholland
Contributor V

That was the problem. Thank you

0 项奖励
回复