MPC5777M can not debug ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777M can not debug ram

ソリューションへジャンプ
4,464件の閲覧回数
1073872596
Contributor I

 

hello!

MCU: SPC5777MK0MVA8

software: S32 v2.1

Debug tool :Multilink Universal FX(PEmicro)

When I debug RAM,S32 does not stop in the “main” function,but stopped in “startup.s”.

Stop in line:e_lis r4, 0xFC05 

;#****************************** Turn off SWTs ********************************
#if defined(DISABLE_SWT2)
;#SWT2
		e_lis	r4, 0xFC05
		e_or2i	r4, 0x8000

		e_li	r3, 0xC520
		e_stw	r3, 0x10(r4)

		e_li	r3, 0xD928
		e_stw	r3, 0x10(r4)

		e_lis	r3, 0x7F00
		e_or2i	r3, 0x010A
		e_stw	r3, 0(r4)
#endif

 

After that, I can only do single-step debugging."Resume(F8)" can't let the program run, only single step.

0 件の賞賛
返信
1 解決策
4,389件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. After burning the flash, debug_ram always has problems.

How should i understand this? So you are loading RAM code into the flash? or?

 

best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,446件の閲覧回数
1073872596
Contributor I

I set breakpoint to main function and hit run, it still only single step one instruction. And, at the begin of Debug RAM, I found the value of "msr" register: 0x9000. It seems wrong.

0 件の賞賛
返信
4,439件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Could you share the project, so I can test it here to see where is the issue?

Did you try it in standalone mode (without debugger) to exclude debugger issue?

best regards,

Peter

0 件の賞賛
返信
4,429件の閲覧回数
1073872596
Contributor I

The board is designed by me with reference to MPC5777M-512DS.

I found the following strange problem:

1. After burning the flash, debug_ram always has problems.

2. For the board that has burned the flash,when debug_ram, you only can run it in a single step, and you can enter the main function. The write operation of some registers in the main function is invalid (for example, SIUL2.MSCR_IO[48].R), and it still keeps the reset value.

3. Board that have never burned flash can be debug normally, and enter the main function, you can single-step operation or resume.Can produce expected results.

0 件の賞賛
返信
4,390件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. After burning the flash, debug_ram always has problems.

How should i understand this? So you are loading RAM code into the flash? or?

 

best regards,

Peter

0 件の賞賛
返信
4,357件の閲覧回数
1073872596
Contributor I

Thank you for your reply.

The MPC5777M can be debugged(debug_ram and debug) online normally, because ERS0 is not properly controlled.

But why my code works fine in the debugger, but fails without debug.

In debug_ram/debug mode, the oscilloscope can capture a square wave on the PD[0].

When I download .ELF into MPC5777M  flash,nothing found on the PD[0].

In debug_ram/debug mode, the register MC_ME_PS0[S_SIUL] = 0x1.

When I download .ELF into MPC5777M  flash,the register MC_ME_PS0[S_SIUL] = 0x0,peripheral is frozen.Therefore, the registers in the SIUL functional unit cannot be operated.

"SIUL2.MSCR_IO[48].R = 0x32840000" can not work.
Is there any way to solve this problem?
 
0 件の賞賛
返信
4,338件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

But why my code works fine in the debugger, but fails without debug.

Debuggers usually disable timer, like watchdogs. therefore you don't have to pay attention to them.

But in standalone application they will cause issues if are enabled and not handled.

Try running some of our example application to see how it is done correctly:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5777M

If you willing to share the application I can have look at it here.

Best regards,
Peter

0 件の賞賛
返信
4,458件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

hello,

From your startup file I can see there is implemented branch to the main.

petervlna_0-1612425492092.png

After that, I can only do single-step debugging."Resume(F8)" can't let the program run, only single step.

So it is not possible to run the code in standalone mode? If you set breakpoint to main function and hit run, does it still only single step one instruction?

Best regards,

Peter

 

0 件の賞賛
返信