MPC5777M Power Up Sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777M Power Up Sequence

1,377 Views
MP
Contributor I

Hello everyone,

i have 2 questions about the power up sequence.

1. Is there an order in which the voltages must be applied to the mcu?

2. Is it required that the VDDDSTBY is present before other voltages are applied?
 (that is unclear in the reference manuel p.182 )

 

0 Kudos
Reply
2 Replies

1,367 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Regarding VDDDSTBY, here is only depends whether STANDBY feature is required or not.  If this voltage is present when VDD_LV is off, SRAM content is preserved. If it is not, SRAM content will not be preserved (will be random after POR).

 

0 Kudos
Reply

1,369 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

The power-on signal is a combination of LVDs monitoring of supplies:
• VDD_LV
• VDD_HV_PMC
• VDD_HV_IO
• VDD_HV_FLA

This signal is released high on exit of the power sequence.

However following limitation exists:

davidtosenovjan_0-1628512227079.png

 

 

0 Kudos
Reply