MPC5777M DMAMUX source slot mapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777M DMAMUX source slot mapping

2,435件の閲覧回数
gelumovileanu
Contributor II

Could anybody provide the MPC5777M DMAMUX source slot mapping? This information is missing in the MPC5777M Reference Manual. Where could I find it?

In chapter 25.3.1 (from MPC5777M Reference Manual) the Channel Configuration register (DMAMUX_CHCFGn) contains a field called SOURCE specifing which DMA source (slot), if any, is routed to a particular DMA channel. See the chip-specific DMAMUX information for details about the peripherals and their slot numbers. But this information I did not find anywhere.

2 返答(返信)

2,259件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

see Table 7-26. DMAMUX peripheral DMA request to input source mapping of the device RM;

https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf 

BR, Petr

2,258件の閲覧回数
gelumovileanu
Contributor II

Hi,

Thank you very much, I did not notice it. I looked for “source slot mapping” like for the other processors.

All the best!

Gelu Movileanu

Von: PetrS

Gesendet: Mittwoch, 6. Juni 2018 06:53

An: Gelu Movileanu <[email protected]>

Betreff: Re: - Re: MPC5777M DMAMUX source slot mapping

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MPC5777M DMAMUX source slot mapping

reply from Petr Stancik<https://community.nxp.com/people/PetrS?et=watches.email.thread> in MPC5xxx - View the full discussion<https://community.nxp.com/message/1021505?commentID=1021505&et=watches.email.thread#comment-1021505>

0 件の賞賛
返信