MPC5777C flash Over-Program Protection issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C flash Over-Program Protection issue

1,433件の閲覧回数
Zhongling_Lang
NXP Employee
NXP Employee

Customer have issue about flash program, the flash blocks cannot program again after enabling CSE secure boot.

After check the C55FMC registers status and found that OPP registers are set with 1 means blocks are protected from being over-programmed.

 

Zhongling_Lang_0-1700123543006.png

So i checked the RM about over-program description which showing over-program protection is enabled by sideband signals. But RM don't mention about this and what reasons caused this problem, customer want to unlock flash and erase/program flash again.

Zhongling_Lang_1-1700123882520.png

 

1 返信

1,403件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

These sidebands signal goes from PASS or TDM modules:davidtosenovjan_0-1700210737881.png

Pay attention to device's RM, section

Chapter 68 - Tamper Detection Module (TDM)

Chapter 67- Password and Device Security Module (PASS)

0 件の賞賛
返信