MPC5777C build problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C build problems

1,796 Views
alphafeely
Contributor II

I have created a empty MPC5777C project , try to build  it , errors below , Help me please

16:06:15 **** Build of configuration Debug for project Hey_MPC5777C_Z7_0 ****
make -j4 all
Building file: ../src/intc_SW_mode_isr_vectors_MPC5777C.c
Building file: ../src/flashrchw.c
Building file: ../src/Vector.c
Building file: ../src/MPC57xx__Interrupt_Init.c
Executing target #3 ../src/flashrchw.c
Executing target #2 ../src/Vector.c
Executing target #1 ../src/MPC57xx__Interrupt_Init.c
Executing target #4 ../src/intc_SW_mode_isr_vectors_MPC5777C.c
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
powerpc-eabivle-gcc "@src/flashrchw.args" -MMD -MP -MF"src/flashrchw.d" -MT"src/flashrchw.o" -c -o "src/flashrchw.o" "../src/flashrchw.c"
powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/MPC57xx__Interrupt_Init.d" -MT"src/MPC57xx__Interrupt_Init.o" -c -o "src/MPC57xx__Interrupt_Init.o" "../src/MPC57xx__Interrupt_Init.c"
powerpc-eabivle-gcc "@src/Vector.args" -MMD -MP -MF"src/Vector.d" -MT"src/Vector.o" -c -o "src/Vector.o" "../src/Vector.c"
powerpc-eabivle-gcc "@src/intc_SW_mode_isr_vectors_MPC5777C.args" -MMD -MP -MF"src/intc_SW_mode_isr_vectors_MPC5777C.d" -MT"src/intc_SW_mode_isr_vectors_MPC5777C.o" -c -o "src/intc_SW_mode_isr_vectors_MPC5777C.o" "../src/intc_SW_mode_isr_vectors_MPC5777C.c"
make: *** [src/intc_SW_mode_isr_vectors_MPC5777C.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [src/flashrchw.o] Error 1
make: *** [src/MPC57xx__Interrupt_Init.o] Error 1
make: *** [src/Vector.o] Error 1

16:06:24 Build Finished (took 9s.329ms)

0 Kudos
Reply
2 Replies

1,635 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify which version of S32DS you used?

Could you please check, if there are not any illegal characters (like some Chinese characters) in path to workspace?

Regards,

Martin

0 Kudos
Reply

1,635 Views
alphafeely
Contributor II

Hey,

S32 Design Studio for Power Architecture

Version: 1.2
Build id: 170613

I have check that  there are not any illegal characters in path to workspace!

thanks!

0 Kudos
Reply