MPC5777C Problem with NCF 42, using debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C Problem with NCF 42, using debugger

2,138 Views
mauriziogreco
Contributor III

Hi, 

has someone an idea about FCCU reaction using TRACE32 ,when the NCF_42 is active?

In the MPC5777C there is the NCF 42: "Lockstep mode Indication of disabled Checker Core or RCCUs. Fault is cleared by clearing the FCCU channel status,FCCU_NCF_Sn[NCFSm]"

I'm working with FCCU active to react to NCF_42.

My SIU_LOCKSTEP.LSE is 1.

When i work on my ECU without TRACE32 (Lauterbach) I don't see any reset action by FCCU.

When i work with TRACE32 (Lauterbach), all is working well until I don't ask "break" on Trace32.

In this case I see the reset action driven by EOUT port of FCCU.

But if I build a new S19 using same code (but in this case keeping disabled NCF 42), all works fine with Lauterbach and also "asking" break on TRACE32.

Where I missing ?

Thanks in advance to all

3 Replies

1,994 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

In debug mode the RCCUs are disabled, therefore you will see this fault.

Make decision block in your SW for disabling NCF42 when debug mode is active, if you want to use lockstep in debug mode.

Peter

1,994 Views
mauriziogreco
Contributor III

Hi Peter, I was only supposing about that.

But now with your confirmation , I feel more certain of solution to be adopted.

Many thanks.

Maurizio


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 Kudos
Reply

1,994 Views
mauriziogreco
Contributor III

Hi, I'm thinking that using debugger the RCCU will be stopped and FCCU start its reaction?

Someone agree with me?

0 Kudos
Reply