Hello!
When I was reading the PFLASH chapter of the reference manual, I saw that the PFLASH_PFCR1 and PFLASH_PFCR2 registers have fields like P1_M2PFE. This field allows the user to enable or disable prefetching from specific masters.

My question is:
If the field P1_M2PFE is set to zero and the master with the logical ID number 2 (FEC) makes a read request, would the data be stored in the mini-cache before it is sent to the FEC or not?
My concern is that even disabling this field, a request from the associated master could evict data in the mini-cache that belongs to other master (e.g., a core).
Best regards,
Matheus