MPC5777C Internal flash memory write issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C Internal flash memory write issue

1,652 Views
prathapvc
Contributor III

Please find the attached file of flash program source code for MPC5777C as per the example code. After executing this code i found that block 30 address locations are getting updated as per the data mentioned in code but again if i want to modify the content of the same address locations i am not able to update it with new data and it is found in disabled state

0 Kudos
Reply
1 Reply

1,646 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, following line does not fit to the the block 30:

C55FMC.SEL2.R = 0x00000002; // select 30 block

 

davidtosenovjan_0-1615477549840.pngdavidtosenovjan_1-1615477580550.png

 

0 Kudos
Reply