MPC5777C Input pad level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C Input pad level

1,569件の閲覧回数
ParthibanPandian
Contributor I

Hi, In MPC5777C, Are there different pad levels for pins configured as input? If so in which section of the reference manual is this mentioned? And is this pad level configurable by software? For example In infineon TC39x there are different levels like AL, TTL3,3 and TTL5

ラベル(2)
0 件の賞賛
返信
1 返信

1,535件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @ParthibanPandian 

The only configurable parameter related to thresholds is hysteresis in corresponding SIU_PCRn register:

lukaszadrapa_0-1728536281237.pnglukaszadrapa_0-1728536281237.png

 

lukaszadrapa_1-1728536288607.pnglukaszadrapa_1-1728536288607.png

 

The threshold are specified like this:

lukaszadrapa_2-1728536309251.pnglukaszadrapa_2-1728536309251.png

 

Regards.

Lukas

0 件の賞賛
返信