Hello!
I am trying to know how many memory banks does the MPC5777C SRAM has, but i did not find any clear information about that in the reference manual or the datasheet. The only information I found is this one, which leads me to conclude that the SRAM has three memory banks, but i am not sure about that.
Could anyone help me with this, please?
Best regards,
Matheus.
Solved! Go to Solution.
Hello,
I know that the MPC5777C has two memory controllers (PRAMC_0 and PRAMC_1), each one connected to different halves of the 512k SRAM.
yes, there are 2 of them. Each one occupying one slave port on XBAR.
I need to know if the 512k SRAM have any internal subdivisions, like different banks, or different SRAM modules (e.g., two 256k SRAM independent modules, each one for one ram controller).
There are two SRAM array modules and 2 PRAM controllers. Each controller has its own XBAR slave port.
Furthermore, is there any PRAMC reference manual of any kind of more detailed documentation?
No, only information which is present in reference manual.
Best regards.
Peter
Hello,
I am not sure what you mean by "banks". But this device has 3 RAM ports.
each module one.
But I do not understand the point here as only initialize ECC on RAM and that's all.
Best regards,
Peter
Hello,
I know that the MPC5777C has two memory controllers (PRAMC_0 and PRAMC_1), each one connected to different halves of the 512k SRAM.
yes, there are 2 of them. Each one occupying one slave port on XBAR.
I need to know if the 512k SRAM have any internal subdivisions, like different banks, or different SRAM modules (e.g., two 256k SRAM independent modules, each one for one ram controller).
There are two SRAM array modules and 2 PRAM controllers. Each controller has its own XBAR slave port.
Furthermore, is there any PRAMC reference manual of any kind of more detailed documentation?
No, only information which is present in reference manual.
Best regards.
Peter
Hello,
Looking at the reference manual:
There are 2 RAM arrays :
1. Standby
2. SRAM
Both of them are on port 2. Standby is in the first part of the addresses.
Are there one SRAM module of 64k and other of 196k to compose the 256k or is there a single 256k SRAM module
From user perspective it really doesn't matter. Such info is not available.
But I expect that there are 2 separate power domains, one for standby is always active.
So the large portion of RAM can be switch off in low power mode.
Best regards,
Peter