MPC5777C FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C FlexCAN

1,438件の閲覧回数
mauriziogreco
Contributor III

Hi all.

Where can be found an example related a injection of fault into flex can RAM, after having enabled ECC ?

Thanks to all.

Regards.

0 件の賞賛
返信
1 返信

1,348件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

we do not have any particular example as the process is quite simple:

To control error injection configure  Memory Error Control Register (CAN_MECR) and set address for error injection:

The error injection is done via Error Injection Address Register (CAN_ERRIAR)

40.4.21   Error Injection Address Register (CAN_ERRIAR)
This register holds the address where error is to be injected. Use the following table to convert from the memory map address to the location in the physical FlexCAN RAM.

regards,

Peter

0 件の賞賛
返信