MPC5777 DSPI Timed Serial Bus (TSB) mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777 DSPI Timed Serial Bus (TSB) mode

Jump to solution
2,905 Views
huayeshen
Contributor I

 

Hi NXP Team,

  I am using the MPC5777M . I am not sure what the DSPI module Timed Serial Bus (TSB) mode in the document . For example:
1.Is TSB used to achieve communication between one host and multiple slaves in DSI or DSI mode?


2.Do data frames and command frames in TSB mode refer to SPI frames and DSI frames, respectively?


3.I see that the selection bit of the command frame in TSB mode is "1", which is written through software. If the command frame is an SPI frame as mentioned in the second question, do I need to turn on the extended SPI mode to write additional selection bits?

Thanks

JAY LEEE

9S[(924Q71TQXS[{4K3]5@O.png

Tags (1)
0 Kudos
Reply
1 Solution
2,845 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Timed Serial Bus (TSB) is a feature you may also see under the name Microsecond Bus (MSC). It is basically SPI communication protocol between MCU and power switch devices established in order to save general purpose output pins:

https://en.wikipedia.org/wiki/Microsecond_Bus

1) There is a dual receiver support, it means there may be used two slaves (two CSs). Pay attention to 49.5.9.1.

2) It is basically CSI mode - command frame is considered as SPI (SW way), data frame as DSI (serialized timer).

3) Not necessarily, it depends on the length of frame.

“The command frame can be written by software, through SPI TX FIFO, using one or two FIFO entries with help of the CONT bit or MCR[XSPI].”

View solution in original post

0 Kudos
Reply
2 Replies
2,846 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Timed Serial Bus (TSB) is a feature you may also see under the name Microsecond Bus (MSC). It is basically SPI communication protocol between MCU and power switch devices established in order to save general purpose output pins:

https://en.wikipedia.org/wiki/Microsecond_Bus

1) There is a dual receiver support, it means there may be used two slaves (two CSs). Pay attention to 49.5.9.1.

2) It is basically CSI mode - command frame is considered as SPI (SW way), data frame as DSI (serialized timer).

3) Not necessarily, it depends on the length of frame.

“The command frame can be written by software, through SPI TX FIFO, using one or two FIFO entries with help of the CONT bit or MCR[XSPI].”

0 Kudos
Reply
2,838 Views
huayeshen
Contributor I

Thank you very much for your answer. I'll go and take a closer look at the documentation.

0 Kudos
Reply