MPC5775K FLEXRAY

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5775K FLEXRAY

2,409 次查看
ronliu
Contributor IV

Dear All,

I'm now working with MPC5775K. Could you please share me some example code of  FlexRay module?

Thanks a lot !

Best regards,

Ron

标签 (1)
标记 (2)
2 回复数

2,085 次查看
martin_kovar
NXP Employee
NXP Employee

Hi Ron,

unfortunately we do not have any Flexray example, but there are two possibilities. First one is AUTOSAR OS and Flexray MCAL driver.

AUTOSAR Software Solutions|NXP

Second one is driver from Vector.

Solutions for FlexRay Networking

But both drivers are under license.

Regards,

Martin

0 项奖励
回复

2,085 次查看
clementchassagn
Contributor II

That's so sad to hear that :smileyhappy:

We contacted Vector, their FlexRay driver is AUTOSAR flavored and also AUTOSAR licensed (which means: reserved to worldwide recognized actors of the automotive industry). In short, there is only one FlexRay implementation, and it is not open to other industries :smileysad:

If the situation changed since last year, we may still be interested in a vanilla implementation of the FlexRay stack, even non-free...