MPC5775E-EVA eTPU DIfferential UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5775E-EVA eTPU DIfferential UART

1,619件の閲覧回数
bchang32
Contributor III

I am looking at the MPC5775E-EVA board. I am trying to figure out if it can handle RS485 UARTs. I see from the function selector that eTPUs can handle UARTs, but I'm not sure if it can handle differential signaling. From looking at the datasheet, it looks like DSPI and MSC can handle differentials (I'm not sure where MSCs are on the board if there are any).

 

Can eTPU handle differential signals (mainly RS485)?

0 件の賞賛
返信
1 返信

1,596件の閲覧回数
johndiener
Contributor IV

eTPU pins cannot handle differential signals directly - external hardware/transceiver would be needed. ASH WARE has produced a version of the eTPU UART function that is more RS-485 capable - e.g. it has driver/transmit enable output capability - see https://github.com/jddiener/UART-eTPU. If there is interest this UART version could be added to the ASH WARE eTPU Code Builder at http://ashware.ddns.net/CodeBuilder/eTPU_code_builder.aspx.

John Diener
0 件の賞賛
返信