MPC5775E-EVA eTPU DIfferential UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5775E-EVA eTPU DIfferential UART

1,620 Views
bchang32
Contributor III

I am looking at the MPC5775E-EVA board. I am trying to figure out if it can handle RS485 UARTs. I see from the function selector that eTPUs can handle UARTs, but I'm not sure if it can handle differential signaling. From looking at the datasheet, it looks like DSPI and MSC can handle differentials (I'm not sure where MSCs are on the board if there are any).

 

Can eTPU handle differential signals (mainly RS485)?

0 Kudos
Reply
1 Reply

1,597 Views
johndiener
Contributor IV

eTPU pins cannot handle differential signals directly - external hardware/transceiver would be needed. ASH WARE has produced a version of the eTPU UART function that is more RS-485 capable - e.g. it has driver/transmit enable output capability - see https://github.com/jddiener/UART-eTPU. If there is interest this UART version could be added to the ASH WARE eTPU Code Builder at http://ashware.ddns.net/CodeBuilder/eTPU_code_builder.aspx.

John Diener
0 Kudos
Reply