MPC5775E 3-phase PMSM Development Kit Design Document

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5775E 3-phase PMSM Development Kit Design Document

2,193 Views
auftrag2021
Contributor III

Hello, 

we plan to buy a MPC5775E 3-phase PMSM Development Kit

I got some design documents below:

auftrag2021_1-1646817220368.png

 

Question1: Can NXP provide the mechanical and electrical datasheet of the PMSM? (not the power board, but the machine)

Question2: Would NXP sell the Power-Board separately as spare part. I have worry about the power board would be easily damaged by the development that we can easily change it with spare part without long time HW debugging

best regards

Siwei

0 Kudos
Reply
3 Replies

2,180 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Question1: Can NXP provide the mechanical and electrical datasheet of the PMSM? (not the power board, but the machine)

No, we are outsourcing the motors from TG drives.

https://www.tgdrives.cz/en/download/3d-models-tgt/tgt2/

Motor is TGT2-0032-30-24/T0PS1K-1M  (0.32Nm, 30V, 0.094 kW, 3000 rpm, 5.2A)

Question2: Would NXP sell the Power-Board separately as spare part. I have worry about the power board would be easily damaged by the development that we can easily change it with spare part without long time HW debugging

No, we do not sell it separately. Only controller card can be bought separately, but power board is sold only as whole kit.

0 Kudos
Reply

2,172 Views
auftrag2021
Contributor III

thanks for quick feedback, but I am confused

the machine type shall be TGN2-0054-30-36

But you give another type number in you feedback. Which one is the correct?

auftrag2021_0-1646902473863.png

 

0 Kudos
Reply

2,161 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It is the one on the web page. I have overlooked this info in order field, and relied on answer from application team.

petervlna_0-1646974202345.png

Best regards,

Peter

0 Kudos
Reply