MPC5775E 3-phase PMSM Development Kit Design Document

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5775E 3-phase PMSM Development Kit Design Document

2,187件の閲覧回数
auftrag2021
Contributor III

Hello, 

we plan to buy a MPC5775E 3-phase PMSM Development Kit

I got some design documents below:

auftrag2021_1-1646817220368.png

 

Question1: Can NXP provide the mechanical and electrical datasheet of the PMSM? (not the power board, but the machine)

Question2: Would NXP sell the Power-Board separately as spare part. I have worry about the power board would be easily damaged by the development that we can easily change it with spare part without long time HW debugging

best regards

Siwei

0 件の賞賛
返信
3 返答(返信)

2,174件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Question1: Can NXP provide the mechanical and electrical datasheet of the PMSM? (not the power board, but the machine)

No, we are outsourcing the motors from TG drives.

https://www.tgdrives.cz/en/download/3d-models-tgt/tgt2/

Motor is TGT2-0032-30-24/T0PS1K-1M  (0.32Nm, 30V, 0.094 kW, 3000 rpm, 5.2A)

Question2: Would NXP sell the Power-Board separately as spare part. I have worry about the power board would be easily damaged by the development that we can easily change it with spare part without long time HW debugging

No, we do not sell it separately. Only controller card can be bought separately, but power board is sold only as whole kit.

0 件の賞賛
返信

2,166件の閲覧回数
auftrag2021
Contributor III

thanks for quick feedback, but I am confused

the machine type shall be TGN2-0054-30-36

But you give another type number in you feedback. Which one is the correct?

auftrag2021_0-1646902473863.png

 

0 件の賞賛
返信

2,155件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It is the one on the web page. I have overlooked this info in order field, and relied on answer from application team.

petervlna_0-1646974202345.png

Best regards,

Peter

0 件の賞賛
返信