MPC574XP can't switch tasks when there is floating-point operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC574XP can't switch tasks when there is floating-point operation

640 Views
darcyxu
Contributor II


If there is floating-point operation in the project, the RTOS cannot switch tasks normally. If the floating-point operation is turned off before and after the open interrupt, it can be normal.
When using floating point arithmetic, which registers are required to be pushed into the stack when the task is switched?
It is best to provide a project with FREERTOS with floating point operations.

0 Kudos
Reply
0 Replies