MPC574XP can't switch tasks when there is floating-point operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC574XP can't switch tasks when there is floating-point operation

1,063件の閲覧回数
darcyxu
Contributor II


If there is floating-point operation in the project, the RTOS cannot switch tasks normally. If the floating-point operation is turned off before and after the open interrupt, it can be normal.
When using floating point arithmetic, which registers are required to be pushed into the stack when the task is switched?
It is best to provide a project with FREERTOS with floating point operations.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)