MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G

2,289 Views
2548903578
Contributor III

I don't quite understand the ME_RUN_PC0..7 register when using MPC5748G. The routine given on the official website is to enable ME_RUN_PC0 = 0x000000fe to enable all modes, but when I look at this register, why are 0-23 bits reserved? Doesn't it make sense to write the lower eight bits? Anyone explain it, thank you very much.

4 Replies

2,130 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Well it is enough to set just 0x000000FC indeed.

Which will represents all modes enabled.

pastedImage_1.png

Doesn't it make sense to write the lower eight bits? Anyone explain it, thank you very much.

By writing 0x000000FC you will write the bits 24 to 29.

I do not understand where do you see the issue?

regards,

Peter

2,130 Views
cholland
Contributor V

I often wondered that myself.

Your writing to register bits that are "read only".

The same goal could have been accomplished with a write of just 0xFC.

In this particular case, the bits are '0' and perhaps it does not matter, which is what I am assuming.

I wonder about cases where the bits are reserved? Would wringing to those bits matter?

0 Kudos
Reply

2,130 Views
petervlna
NXP TechSupport
NXP TechSupport

No,

once the bits are read only you cant write to them, The write will be ignored.

regards,

Peter

2,130 Views
2548903578
Contributor III

I already understand, thank you

0 Kudos
Reply