MPC5748G uSDHC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G uSDHC

2,067 Views
491844366
Contributor I

Hello! I am confused about uSDHC on MPC5748G  for some days,the response from CMD1 can be seen by an oscilloscope, but the processor  just can't catch it,somebody help me plaese!
Thank you!

Tags (3)
0 Kudos
Reply
2 Replies

1,905 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Could you explain issue you are seeing more closely?

I am not able to tell you where is the issue from such brief explanation of issue.

regards,

Peter 

0 Kudos
Reply

1,905 Views
491844366
Contributor I

Thank you for your reply!

 

After the USDHC is initialized, CMD0 instruction is sent to the EMMC to make the  EMMC enter IDLE mode.

Send CMD1 instruction to obtain the OCR register information of the EMMC. MPC5748G’s register of response have not received value, the Command Complete (CC) bit is not set, and the Command Inhibit (CIHB) bit is 0. However, it can be seen from the oscilloscope that the EMMC has a response waveform after receiving the CMD1 signal.

 The source code is attached.

Could you tell me what’s wrong with the configuration?

Looking forward to your reply.

Thank you!

0 Kudos
Reply