MPC5748G modes selection RUN0-RUN3, DRUN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G modes selection RUN0-RUN3, DRUN

1,475 Views
dbabu_ele
Contributor I

Hi All,

Currently i started working with MPC5748G LCEVB.

I want run my application code for FlexCAN0 in core0 and other piece of code in core1 independently.

Can anyone please help me for below questions. 

1. I would like to know when to use multi cores for MPC5748G controller?

2. In which scenario we have to use mode DRUN?

3. In which scenario we have to use modes RUN0-RUN3?

4. Shall we use core0 in DRUN and core1 in modes RUN0-RUN3?

 

Thanks in advance.

regards,

Babu Dudekula

Tags (1)
0 Kudos
Reply
1 Reply

1,368 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

1. I would like to know when to use multi cores for MPC5748G controller?

When you need more performance than single core offers. Otherwise you should go with single core as each active core has significant current consumption.

2. In which scenario we have to use mode DRUN?

Usually DRUN is used for initialization of device - DRUN = default run

3. In which scenario we have to use modes RUN0-RUN3?

For application execution

4. Shall we use core0 in DRUN and core1 in modes RUN0-RUN3?

No, there is only one mode entry module and selected mode is common for all cores.

Peter

0 Kudos
Reply