MPC5748G debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G debug problem

2,152件の閲覧回数
chenxiubo
Contributor III

Hi,

      I'm using PE to debugg  MPC5748G project ,but there is problem in progress,177546_177546.jpg11.jpg177547_177547.jpg1.jpg

 I powed down and powed up the power, pressed  'OK' in the first picture, but there is the other problem in the second

picture. I pressed  'Retry ' ,and   the first problem appeared again.......

How to solve theses problems?

ラベル(1)
3 返答(返信)

1,988件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

did not you accidentally turn off the power supply or push reset button during the downloading your code to the microcontroller?

Have you correctly installed and updated PEMicro drivers?

Regards,

Martin

1,988件の閲覧回数
chenxiubo
Contributor III

Hi, Martin Kovar

 The hardware hasn't  push reset button,and  I didn't  turn off power when downloading code.

  I  guess the mcu has been secured ,and how to unsure the mcu  for S32 IDE?

  Or is there any problems?How to solve it?

  Best  regards.

  tom_chen

0 件の賞賛
返信

1,988件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Tom,

if you use only S32 Design Studio, it is nearly impossible to secure the device. S32DS does not modify UTEST flash area.

At first, check you have correctly installed and update PEMicro drivers.

Which debug probe you use?

If you use Multilink Universal or Multilink Universal FX, please disconnect jumper J5 in debug probe.

Which version of S32DS you use? version 1.0 or 1.1?

What is your microcontroller mask?

Did you try to use another microcontroller?

Regards,

Martin