MPC5748G SPI write/read SDK function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G SPI write/read SDK function

1,128件の閲覧回数
kimdukyu
Contributor II

Hi.

I am using SPI example program with version S32_SDK_S32PA_RTM_3.0.3.
If you look at the API, there is no write/read function, and write/read is performed at once with the transfer function.
I want to write write and read separately, but I wonder if there is a corresponding API.
If not, please answer how to implement it.

Thank you.

0 件の賞賛
返信
1 返信

1,115件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Dukyu,

it's the nature of SPI interface. While SPI master sends data to slave device, the slave device always sends data back to the master at the same time. So, there's no API for separate operations.

The only workaround is:

- if you want to only send something from master to slave, ignore the data which are send back by slave

- if master device is required only to read something from slave, send some dummy data to slave, so the master will generate clocks needed to clock the data out from the slave

Regards,

Lukas

0 件の賞賛
返信