MPC5748G - PORST Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,986件の閲覧回数
michaelm
Contributor I

Hi,

 

with the help of the reference manual I found out what to do with the Porst Pin when using an external 1.25V supply. But what to do with the PORST Pin when using the NPN ballast transistor for providing the 1.25V?

Connect PORST to the 1.25V? Connect PORST to VDD_HV? Leave PORST floating?

(I'm using the MPC5748G)

 

Thank you in advance,

 

Michael

ラベル(1)
1 解決策
1,805件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when using the internal core voltage regulator and external ballast transistor, it is recommended to pull the PORST pin to VDD_HV_A via 10k resistor.

Best Regards,

Lukas

元の投稿で解決策を見る

1 返信
1,806件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when using the internal core voltage regulator and external ballast transistor, it is recommended to pull the PORST pin to VDD_HV_A via 10k resistor.

Best Regards,

Lukas