MPC5748G Flash Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G Flash Problem

19,579 Views
bdn
Contributor III

Hi,

I'm experiencing a problem with MPC5748G Eval-Kit.

I flashed the controller via JTAG with the pemicro Multilink Universal FX. During that progress I accidently hit the reset button. I don't know when exactly the reset happened but I think during erasing. The MPC5748G now stays in reset mode (red LED, D1 stays on). I cannot connect via JTAG.

 

Now the question is: Is there any way to revive the controller? Do I need another debug tool (lauterbach or iSYSTEM)?

 

Thanks and regards,

Bernhard Dielhenn

Labels (1)
31 Replies

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

Use Lauterbach debugger is the easiest way how to connect, but there is another workaround.

Download and install CodeWarrior

http://cache.nxp.com/lgfiles/devsuites/PowerPC/CW55xx_v2_10_SE.exe

Download this patch and update the CodeWarrior according to Readme.txt file

http://www.pemicro.com/faqs/faq_view.cfm?id=211

Run cw_progppcnexus.exe and click connect.

pastedImage_1.png

Popup window with reset escalation information appears. Do power on reset (switch board off and on and click OK).

After that, window with choosing algorithm appears. Click cancel.

pastedImage_2.png

Now double click Reset chip.

pastedImage_3.png

Popup window with reset escalation information appears again. Do power on reset and click OK. Now you should be able to connect via PeMicro until next power on reset.

Please write me back if it helps you.

Regards,

Martin

0 Kudos
Reply

12,126 Views
virbhadrahankun
Contributor I

Hi Martin, 

# Flash programming error due to CRC-16 mismatch file to device 

I have the similar issues described below.

 

I am using S32 design studio and openSDA debudder to dubug sample application. It worked for 2 3 hours and after that the board is giving problem to load the programme.

It is stucks at verification of block. have a look at screen shot. 

 

 

 

Connection from "127.0.0.1" via 127.0.0.1
Copyright 2017 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5000 -resetÌ

CMD>RE

Initializing.
MPC574xC Device detected. 
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&E\nxp_mpc5748g_1x32x1520k_cflash.pcp

Initializing.
MPC574xC Device detected. 
Initialized.

;version 1.05, 06/26/2017, Copyright P&E Microcomputer Systems, www.pemicro.com [5748G_6080k]

;device NXP, MPC5748G, 1x32x1520k, desc=CFlash

;begin_cs device=$00F90000, length=$005F0000, ram=$40000000

Loading programming algorithm ... 

WARNING - Selected .PCP file has been modified. CRC16 = $5A63 
Done.
CMD>VC
Verifying object file CRC-16 to device ranges ... 
block 00FA0000-00FA0007 ...

Please reply we have lost such 5 Devkits  because this issue

regards,

Virbhadra H.

0 Kudos
Reply

12,126 Views
yukunwu
Contributor III

Hi Martin,

       I have also met this problem .There is a window poped up when i debugged the MPC5748G.

      捕获.JPG

     I built the project in S32D and used the Opensda debugger.

      Could you tell me what's the reason of this situation? and how to sovle it ?Thanks very much!

Best Regards,

Yukun Wu.

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi,

first of all thank you very much for your answer. This is what I did so far:

- CodeWarrior installed

- PE Micro patch installed

- cw_progppcnexus.exe crashed

- I have two driver versions for PE Multilink FX

     - 10.1.0.0 [26.01.2011]

     - 12.2.0.0 [26.10.2015]

- after choosing the newer one, cw_progppcnexus.exe starts and after clicking connect I get the message refering reset escalation. When I power cycle the board and confirm the reset escalation message, the connection manager window comes up again. So I still cannot connect it.

Any idea what I can try?

Or as plan B, is there any way to purchase another PPC5748GMMN6A 1N81M? I really need a running Eval-Kit. This board had five weeks delivery time.

Thanks and regards

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

this is strange. Which IDE (or tool) you use for flashing program? Is it S32 Design Studio? This issue could be caused by some active debug session. Just to make sure, did you download this patch?

http://www.pemicro.com/downloads/download_file.cfm?download_id=463

If you use S32DS, please kill pegdbserver_power_console.exe process and also powerpc-eabivle-gdb.exe process. Both these processes can block the connection. Kill both processes and restart cw_progppcnexus application.

If you do not use S32DS, please write me, which tool you use.

Also you can use PEFirmwareUpdater which is part of PEDrivers you can download from PEmicro website. This app is able to update PE Multilink FX firmware.

http://www.pemicro.com/downloads/download_file.cfm?download_id=346

I tried to do whole process mentioned above with USB-ML-PPCNEXUS and also with USB-ML-UNIVERSAL-FX and it works with both.

So please try the steps above and write me back if it helps.

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi Martin,

I downloaded and installed the patch CW210_patch_Qorivva.zip.

I'm using S32DS and there are none of the mentioned processes running.

The PE Micro USB Multilink Universal FX has the latest firmware 9.40 on it. cw_progppcnexus detects that.

Thank you and regards

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please send the following screen from your side?

pastedImage_0.png

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

When I start cw_progppcnexus:

PEMicroConnMan1.png

And after Connect and power cycle:

PEMicroConnMan2.png

When I click on Reset, the yellow LED lights two times but the red one (from MCU) stays red all the time. So I think the MCU doesn't recognize the reset from PE Micro.

In S32DS I had to set up a Delay after Reset and before communication but this didn't help here.

Regards

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

I think I finally found the problem (thank to my colleague). Please disconnect the jumper JP10 in Multilink Universal which is used for independent power supply. Now it should work correct.

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi Martin,

thank you again for your efforts!

The jumper JP10 (on PE Multilink) was not connected all the time. The power supply comes only from the eval board. So power off and on at the eval board will remove power supply from the MPC5748G. During powercycle the red led switches off. But not after Reset from JTAG, maybe that wasn't clear after my last post.

I have no idea what else I can test. Is there any way to purchase the PPC5748GMMN6A 1N81M? Or would an iC5500 from iSYSTEM be helpful? I could get an Eval Trace probe for limitted time.

Thank you and regards

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

from your last post I am little bit confused. After power on reset (without debugger), is D1 on or off (I suppose on)?

If D1 turns off (tell me the condition when D1 turn off, if ever), are you able to connect via S32DS?

About iC5500 i do not know this system, so I am not able to tell you any relevant information, but you can try.

New micro you can by at the following link:

MPC574xB/C/D/G|32-bit MCU|Gateway|NXP

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi Martin,

sorry for confusing you. D1 is on all the time. I wanted to say, it switches off when I turn off the power supply from the eval board. This indicates for me that PE Multilink does not supply the board with power (JP10 is not set).

Usually if I enter the BDM mode the red LED would turn off. But I cannot enter BDM and the red LED stays on.

S32DS tells "The target may have entered reset escalation. Please power cycle the board." After doing that the connection manager appears again. After triyng to connect, reset escalation message comes up again and so on.

As I see it, there is no MAPBGA 324 pagacke available. So I would have to buy another Daughterboard.

Regards

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

maybe one last desperate attempt. Please look at this thread, but I suppose you have done this step.

How to debug multicore with S32 Design studio

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi Martin,

as I sayd I already tried to add a delay time. That worked for normal flashing but not here.

I think I cannot revive it with these tools (PE Micro + S32DS or CodeWarrior).

But thank you for helping.

Regards

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

if you discovered the issue somehow (accidentally ;-) ), please write me back. I would like to know the root cause of the issue, because I tried 3 different debug probes and I was able to connect with all of them.

I regret we were not able to solve the issue, because I think the device is not censored (S32DS does not modify UTest flash). It remains a mystery for me, why you are not able to connect.

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi,

I have now the lauterbach debugger on my desk. I tried the demo script and it says "debug port fail".

What can I try next?

Regards

Bernhard

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

power up your board, and start Trace32. Now you are not able to attach - it is correct.

Click MPC5XXX->Tools->Halt core at power-on reset.

pastedImage_0.png

Now you should see following window:

pastedImage_1.png

Switch off the board, wait a while (a few seconds) and switch on the board. Now LED D1 has to be off.

Now you should see something like that (the window with code you show using command B::list, or click View->List Source):

pastedImage_2.png

Now click MPC5XXX->Tools->Program Flash(Dialog) and choose the elf you want to flash.

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi Martin,

thank you for your quick and detailed reply.

After powerup the red LED (D1) stays on and Trace32 still says "debug port fail" and "unexpected error".

Regards,

Bernhard

0 Kudos
Reply

12,133 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

could you please send me screen of Message Area? Please click View->Message Area and send me the screen of the window.

Regards,

Martin

0 Kudos
Reply

12,133 Views
bdn
Contributor III

Hi Martin,

here's the screen:

Message_Area.png

What does OSR and JCOMP mean?

Regards,

Bernhard

0 Kudos
Reply