MPC5748G CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G CAN

Jump to solution
122 Views
徐工2024
Contributor II

Hello, I would like to ask some questions about can0 receiving interrupt, I implemented is to receive all can id messages:
Question 1: My program does not know why it can only enter the interrupt if MB[5] interrupt is enabled, and why reading MB[0] can read the correct message at this time. If I enable MB[0] interrupt, I cannot enter the receive interrupt, why? I read the message content of MB[0] and should also enter the MB[0] interrupt, here is my code.

2024_0-1742542662797.png

 

Tags (1)
0 Kudos
Reply
1 Solution
91 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

A1) as I wrote MB flags change meaning when RXFIFO is used.

PetrS_0-1742556904913.png

So if there is new message in RXFIFO MB5 flag is set, if corresponding IMASK1 bit is set, interrupt is generated.

2) RFFN specifies how many filter elements will be used in RXFIFO. This will determine which MBs will be used by RXFIFO engine and ID Filter table, which MBs remains to be used for general TX or RX operation. Also specified how many filter elements will use individual masking registers, rest will FIFO global mask register. 

3) the CPU can read the message from RXFIFO by accessing the output of the FIFO  (MB0) as a Message Buffer and the CAN_RXFIR register and then clear the interrupt (MB5 flag). If there are more messages in the FIFO the act of clearing the interrupt (MB5 flag) updates the output of the FIFO with the next message and update the CAN_RXFIR with the attributes of that message, reissuing the interrupt to the CPU. Otherwise, the flag remains negated.

BR, Petr

View solution in original post

0 Kudos
Reply
4 Replies
95 Views
徐工2024
Contributor II

Thank you for your reply. Yes, I enabled RX FIFO, but I still have the following problems:
Question 1: According to the manual, if RX FIFO is enabled, MB[0~5] is occupied by RX FIFO (and I did not set the RFFN bit), but why MB[5] can enter the interrupt when sending data to CAN?MB[5] Isn't it occupied? Is there some kind of drinking relationship here?
Question 2: I don't quite understand the meaning of the RFFN figure, can you answer it for me?

2024_0-1742555641502.png

 


Question 3: Why does this project need to read MB[0] of data after using MB[5] to enter the interrupt? Data projects that read MB[5] will go wrong, why?
Looking forward to your reply!
This is my project source code.Thank you!

0 Kudos
Reply
92 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

A1) as I wrote MB flags change meaning when RXFIFO is used.

PetrS_0-1742556904913.png

So if there is new message in RXFIFO MB5 flag is set, if corresponding IMASK1 bit is set, interrupt is generated.

2) RFFN specifies how many filter elements will be used in RXFIFO. This will determine which MBs will be used by RXFIFO engine and ID Filter table, which MBs remains to be used for general TX or RX operation. Also specified how many filter elements will use individual masking registers, rest will FIFO global mask register. 

3) the CPU can read the message from RXFIFO by accessing the output of the FIFO  (MB0) as a Message Buffer and the CAN_RXFIR register and then clear the interrupt (MB5 flag). If there are more messages in the FIFO the act of clearing the interrupt (MB5 flag) updates the output of the FIFO with the next message and update the CAN_RXFIR with the attributes of that message, reissuing the interrupt to the CPU. Otherwise, the flag remains negated.

BR, Petr

0 Kudos
Reply
114 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

your code only shows you enabled interrupt for MB[4] (IMASK1=0x10). It does not indicate, how MBs are configured and used. Commented code  and last MCR writing indicates RXFIFO is enabled. When RFEN is set, MBs 0 to 5 cannot be used for normal reception and transmission because the corresponding memory region (0x80-0xDC) is used by the FIFO engine as well as additional MBs (up to 32, depending on CAN_CTRL2[RFFN] setting) which are used as Rx FIFO ID Filter Table elements.
Low mask bits in IMASK1 also change its meaning, see more in 44.5.8 Rx FIFO chapter of the device RM.

BR, Petr

0 Kudos
Reply
94 Views
徐工2024
Contributor II

Sorry, there is an error in the project. The if judgment in can0_isr should be CAN0

0 Kudos
Reply