MPC5748G Adding DCF record

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G Adding DCF record

13,524件の閲覧回数
rahulramakrishn
Contributor III

Hi

I am using S32DS to debug MPC5748G. I want to enable the HSM module in MPC5748G. I found that in order to activate the HSM module, I need to set the HSE bit via DCF record. But I didn't found a way to set the DCF record. How can I access the DCF record in order to enable the HSM module in MPC5748G?

Regards

Rahul Ramakrishnan

25 返答(返信)

2,754件の閲覧回数
rahulramakrishn
Contributor III

The first 64 bits that is not written. The location can be identified by

the sequence FFFFFFFF.

In your case 00400380.

If u able to update the DCF record please inform me.

On Jul 3, 2018 8:14 PM, "[email protected]" <[email protected]>

0 件の賞賛
返信

1,940件の閲覧回数
yashkhatri0291
Contributor II

I tried writing on 380, 390 and even 400 but there was no success.

It cannot be written over those records. Do we need to take some read/write permission in HSM or is it given to us automatically. I want some insights over the HSM_Control register(A3F8_0000), wherein 2 keys are mentioned. Where do we use those keys?

I insist your and Peter's help in this subject.

0 件の賞賛
返信

1,940件の閲覧回数
yashkhatri0291
Contributor II

sorry the address is 0xA3F84000.

0 件の賞賛
返信

1,940件の閲覧回数
rahulramakrishn
Contributor III

I also stuck in this problem. I didn't found any way to overcome this. If

you found anything please let me know.

On Jul 4, 2018 4:08 AM, "[email protected]" <[email protected]>

0 件の賞賛
返信

1,940件の閲覧回数
rahulramakrishn
Contributor III

Hi

Thank for your support. I am new to this field and this is the first time I

am working with a board. Thank for your time.

Regards

Rahul Ramakrishnan

0 件の賞賛
返信