MPC5748C Re-initializes Flexcan

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5748C Re-initializes Flexcan

跳至解决方案
2,578 次查看
xiha
Contributor II

My projects are based on Flexcan and ETHERNET.Now I'm going to re-initialize Flexcan after receiving the command over the network,but I can't restart FlexCan successfully.The driver isn't normal.CANFD communication is error.The log of CANFD sender, printf ErrorFrame.The code is as follows:

flexcan_user_config_t my_canCom1_InitConfig0 = {
    .fd_enable = true,
    .pe_clock = FLEXCAN_CLK_SOURCE_OSC,
    .max_num_mb = 16,
    .num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,
    .is_rx_fifo_needed = false,
    .flexcanMode = FLEXCAN_NORMAL_MODE,
    .payload = FLEXCAN_PAYLOAD_SIZE_64,
    .bitrate = {
        .propSeg = 7,
        .phaseSeg1 = 5,
        .phaseSeg2 = 4,
        .preDivider = 1,
        .rJumpwidth = 1
    },
    .bitrate_cbt = {
        .propSeg = 11,
        .phaseSeg1 = 3,
        .phaseSeg2 = 3,
        .preDivider = 0,
        .rJumpwidth = 1
    },
    .transfer_type = FLEXCAN_RXFIFO_USING_INTERRUPTS,
    .rxFifoDMAChannel = 0U
};
flexcan_data_info_t dataInfo =
{
  	.data_length = 64U,
  	.msg_id_type = FLEXCAN_MSG_ID_STD,
//	.msg_id_type = FLEXCAN_MSG_ID_EXT,
  	.enable_brs  = true,
  	.fd_enable   = true,
  	.fd_padding  = 0U
};

FLEXCAN_DRV_Deinit(INST_CANCOM1);
FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);

FLEXCAN_DRV_InstallEventCallback(INST_CANCOM1,my_callback_event,NULL);
/* Configure RX message buffer with index RX_MSG_ID and RX_MAILBOX */
FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, RX_MAILBOX, &dataInfo, 0u);
FLEXCAN_DRV_SetRxMbGlobalMask(INST_CANCOM1,FLEXCAN_MSG_ID_STD,0);

 If anyone can help to solve this problem?Thanks you very much!

0 项奖励
回复
1 解答
2,551 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can use FLEXCAN_DRV_SetBitrate and FLEXCAN_DRV_SetBitrateCbt for that, but changing bitrate requires all nodes on bus follow that too, otherwise you get error for further communications.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,560 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

why is the deinit/init needed in fact? What kind of error is detected on sender side?
You can inspect FlexCAN module registers to know if Normal mode is entered and no errors are detected during message reception. Not sure if module also transmit anything.

BR, Petr

0 项奖励
回复
2,556 次查看
xiha
Contributor II

Because I wanted to send commands to the MCU over the network and then change the baud rate of its CANFD communication, I used DeInit and Init to change the CANFD baud rate.

Thanks for your advice. I'll try.

0 项奖励
回复
2,552 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can use FLEXCAN_DRV_SetBitrate and FLEXCAN_DRV_SetBitrateCbt for that, but changing bitrate requires all nodes on bus follow that too, otherwise you get error for further communications.

BR, Petr

0 项奖励
回复
2,545 次查看
xiha
Contributor II

Your advice is very useful, thank you!!! \ ^_^ / \ ^_^ / \ ^_^ /

0 项奖励
回复