MPC5746C breakpoint in the Interrupt Service Routine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C breakpoint in the Interrupt Service Routine

2,504 Views
cholland
Contributor V

Hi,

I have some strange happenings going on.

When I enable a breakpoint in an ISR, the code immediately stops at the breakpoint.

It doesn't seem to be caused by the code, but only because of the breakpoint being set.

I set the breakpoint at random times. Like 3,4,5,6,7 minutes in and it's the same.

Somehow enabling a breakpoint is causing the ISR to be called?

I have a GPIO pin I enable for an interrupt.

SIUL2.MSCR[PC4].R = 0u;

SIUL2.MSCR[PC4].B.IBE = 1u;

SIUL2.IMCR[674-512].B.SSS = 1u;

SIUL2.IFEER0.B.IFEE18 = 1u; /*falling edge event enabled (As per HITS Active Level = Low) */

/* SIUL2.IFER0.B.IFE18 = 1u; */ /*enable interrupt filter */

SIUL2.IRER0.B.EIRE18 = 1u; /*enable interrupt */

void SIUL_EIRQ_C(void)

{

   if(SIUL2.ISR0.B.EIF18) /* TP 394 */

   {

   /* Clear IRQ 18 */

   SIUL2.ISR0.B.EIF18 = 1;   <-- When I enable breakpoint here, the code stops immediately

   WDTC++;                           <-- Counter is 0.

   }

}

Thanks

4 Replies

2,131 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify which IDE and version you use?

It is strange behavior and break point adding should not affect the code this way.

Regards,

Martin

2,131 Views
cholland
Contributor V

So, somehow the breakpoint is tied to IRQ 18.

I can set the breakpoint in other parts of the code and whenever I do, only IRQ 18 triggers.

I set counters to monitor how many times all the IRQs trigger. When I break in other parts of the program,

I only see the IRQ 18 counter increase.

So it doesn't matter where the break point is set, I just know that each time the breakpoint is set, IRQ 18 triggers.

Thanks,

0 Kudos
Reply

2,131 Views
cholland
Contributor V

Hi Martin,

I went back and setup ISRs for SIUL_EIRQ_0_7, SIUL_EIRQ_8_15 and SIUL_EIRQ_24_31.

None of the other ISRs have a problem. It only seems to happen with SIUL_EIRQ_16_23.

I changed the ISR names in hopes something would change, but nothing did.

(uint32_t) &SIUL_EIRQ_0_7, /* Vector # 243 SIUL EIRQ [0-7] - SIUL Combined External Interrupt */

(uint32_t) &SIUL_EIRQ_8_15, /* Vector # 244 SIUL EIRQ [8-15] - SIUL Combined External Interrupt */

(uint32_t) &SIUL_EIRQ_16_23, /* Vector # 245 SIUL EIRQ [16-23] - SIUL Combined External Interrupt */

(uint32_t) &SIUL_EIRQ_24_31, /* Vector # 246 SIUL EIRQ [24-31] - SIUL Combined External Interrupt */

Also, it doesn't matter where I add the breakpoint.

void SIUL_EIRQ_16_23(void)

{

   if(SIUL2.ISR0.B.EIF18) /* TP 394 */

   {

   /* Clear IRQ 18 */

   SIUL2.ISR0.B.EIF18 = 1;

   WDTC++;

   }

}

0 Kudos
Reply

2,131 Views
cholland
Contributor V

S32 Design Studio for Power Architecture

Version: 2017.R1

Build id: 171018

(c) Copyright Freescale Semiconductor 2016. All rights reserved.

(c) Copyright NXP 2017.

0 Kudos
Reply