Hi,
I use the official demo, but I don't know why, when running to the PIT register operation, the program jumps to IVOR1_Handler. I have this problem with PIT Demo or CAN Demo alone. What conditions might cause this problem? At present, 8 pieces of MPC5746C in the hand have such problems.
Hi,
Thank you very much for your answer. I seem to have found the problem. Currently, there is no OSC32K external pin in the MCU of the MPC5746C 100MAPBGA, and MC_ME.DRUN_MC.SXOSCON is enabled in the Demo of the SDK, but it does not judge and wait for MC_ME.GS. The .B.S_MTRANS bit is set to 0, so the program jumps to the IVOR1_Handler interrupt when the PIT register is manipulated.
It seems that the officially provided Demo Code does not distinguish the 100MAPBGA of the MPC5746C from other Pin packages