Progrem flash for MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Progrem flash for MPC5748G

Jump to solution
2,721 Views
gj3526
Contributor III

Hi all:

    I'm designing a BootLoader that needs to progrem SREC files to flash, but there's a part of the SREC file as follow. if progrem eight words once,it will break as follow when data is not in one flash page.if progrem one word by one word ,when program next eight  words, it will auto change one word which just has progremd.how can I deal with it.

the srec file:

S3150100737C006A006A006A0014001500160054000A1F

program eight words

0x0100737C  006A006A FFFFFFFF FFFFFFFF FFFFFFFF//after program 006A006A it will break

program one words

0x0100737C  006A006A 006A0014 00150016 00000000 /// when program 0x0100738C  it will be set to 00000000

sdk code:

            for (sourceIndex = 0U; sourceIndex < temp; sourceIndex++)
            {
                /* Programming write */
                *(volatile uint32_t *)dest = *(volatile uint32_t *)source;
                /* Update dest, size, source index */
                dest += C55_WORD_SIZE;
                source += C55_WORD_SIZE;
                size -= C55_WORD_SIZE;

                /* Is it time to do page programming?  */
                if(0U == (dest % FLASH_C55_PROGRAMABLE_SIZE))
                {
                    break;//////////////////////////////////////////  it will break when data in two pages
                }
            }

Best Regards,

gong jun

Tags (1)
1 Solution
2,621 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

here is an explanation of the behavior:

pastedImage_1.png

Regards,

Lukas

View solution in original post

2 Replies
2,622 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

here is an explanation of the behavior:

pastedImage_1.png

Regards,

Lukas

2,621 Views
gj3526
Contributor III

hi Lukas,

It seems that I can only change the SREC file,Thank you very much!

Best Regards,

gong jun

0 Kudos
Reply