MPC5746 Internal TVS current level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5746 Internal TVS current level

跳至解决方案
1,475 次查看
RheaGao
Contributor I

Hi,

 I am using SPC5746R chip to design the minimum system with 1.25V using the following same circuit. During the debugging process, I found that 5746 would not work if I did not add Clv 1uF buffer capacitor to write the program with 200M main frequency. Specifically, I was stuck in the clock initialization and could not pass.  What mechanism triggers the microcontroller to cause this?  Thanks!

 

 

0 项奖励
回复
1 解答
1,455 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Rhea,

 

Do you mean that 1uF capacitor is the only one at VDD_LV? The specification says that minumum capacitance is 4.7uF:

lukaszadrapa_0-1651474177761.png

And it’s minimal value. It should be validated by user for given application.

It is also recommended to use Progressive Clock Switching feature to avoid current spikes. Search for „Progressive Clock Switching“ in the reference manual for details.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,456 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Rhea,

 

Do you mean that 1uF capacitor is the only one at VDD_LV? The specification says that minumum capacitance is 4.7uF:

lukaszadrapa_0-1651474177761.png

And it’s minimal value. It should be validated by user for given application.

It is also recommended to use Progressive Clock Switching feature to avoid current spikes. Search for „Progressive Clock Switching“ in the reference manual for details.

Regards,

Lukas

0 项奖励
回复