MPC5744P disable nexus auxiliary interface when using Serial Aurora

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P disable nexus auxiliary interface when using Serial Aurora

1,323 Views
chosp
Contributor III

Hello

I have some digital outputs connected to MSEO[0] and MSEO[1] pins.

Debugging with LAUTERBACH TRACE32 using the Serial Aurora connection, I am not able to control those pins unless I disable NEXUS.

According to the documentation, those pins correspond to functionalities employed with Parallel Nexus.

Is there any way I can disable those functionalities while retaining the Nexus functionality on its Serial Aurora configuration?

thank you

0 Kudos
Reply
1 Reply

1,284 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The function of the trace pins is usually directly bound to enabling of the trace. If the SIUL does not allow overriding the setting, then I am afraid it is not possible to use trace MSEO pins at the same time.

Unless there is some undocumented feature I don't know of...

Best regards,

Peter

0 Kudos
Reply