MPC5744P dev board uart example does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P dev board uart example does not work

Jump to solution
2,355 Views
ahmedHasan
Contributor I

Hello 

i'm trying the example UART_PAL_ECHO for this kit 

i can't get any thing on the terminal i'm using REV E

0 Kudos
Reply
1 Solution
2,343 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I tried uart_pal_echo example from SDK 3.0.3 on DEVKIT revE and it seems to be working fine, as per example description in doxygen file.

PetrS_0-1651229625052.pngPetrS_0-1651229625052.png

BR, Petr

View solution in original post

0 Kudos
Reply
3 Replies
2,334 Views
ahmedHasan
Contributor I

Hmmmmm 

while trying the example uart echo in matlab i had to change from serial 1 to serial 0 in config box to get it working 

should i change it also when i use the example in SDK in s32 ?

0 Kudos
Reply
2,295 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

on DEVKIT-MPC5744P revE LINFlexD_0 using pins PB2/PB3 is connected to K20 MCU which serves as serial-to-USB module on the board. So LINFlexD_0 need to be selected in uart_pal component and PB2/PB3 pins configured in pin_mux component. But it is done in demo code.

BR, Petr

0 Kudos
Reply
2,344 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I tried uart_pal_echo example from SDK 3.0.3 on DEVKIT revE and it seems to be working fine, as per example description in doxygen file.

PetrS_0-1651229625052.pngPetrS_0-1651229625052.png

BR, Petr

0 Kudos
Reply