Dear Sir
We are now facing a problem in our own board which is using MPC5744P IC.
When I was using debug mode, the program runs normally and the function is correct,
but after leave debug mode, let the MCU runs as stand alone(also reset the power), the program cannot run normally, and the function is incorrect.
We had checked the 40MHz oscillator and VDD_LV_PLL0 , these two pin provides the correct voltage.
Do you have any suspect of this kind of issue or how can we troubleshooting to let the stand-alone mode succeed?
Thanks!