MPC5744P cancasexl bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P cancasexl bootloader

1,450 次查看
johnjiang888888
Contributor I

NXP MPC5744P

rbf: MPC5744P_S32DS_UART1_CAN0.rbf

tools:cancasexl+RAppID

description:The program can be loaded successfully,But it doesn't work,Why?

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

1,319 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

did you follow these instructions in the user manual?

pastedImage_1.png

And this is from the release notes:

pastedImage_2.png

This is the most common reason. The application will not work if the steps above are not implemented.

Regards,

Lukas

0 项奖励
回复

1,319 次查看
johnjiang888888
Contributor I

09C34E46-A636-40e5-A649-E835C97A0507.png

hello,where is my problem?

thanks

0 项奖励
回复

1,319 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's not about the settings of Rappid tool or about the RBF file. It's about the application which you are going to download by the bootloader. You need to implement the steps mentioned above.

Regards,

Lukas

0 项奖励
回复

1,319 次查看
johnjiang888888
Contributor I

Problem has been solved,Thank you

0 项奖励
回复