MPC5744P SWT keep running in STOP0 mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P SWT keep running in STOP0 mode

Jump to solution
4,909 Views
hangxie
Contributor III

1. config the SWT timeout to 1 second with drv_cpu_initswt().

void drv_cpu_initswt(uint32_t Timeout)
{
/* remove the SWT Soft lock */
SWT_0.SR.R = 0xC520;
SWT_0.SR.R = 0xD928;
/* Wait for solf-lock bit */
while (SWT_0.CR.B.SLK == 0x1);
/* Disable SWT_0 */
SWT_0.TO.R = 0x0F42400 * Timeout; //
SWT_0.CR.R = 0xFF00010E; // STP = 1, FRZ = 1, WEN = 0
}

2. after all init finished, enable the swt with drv_cpu_enableswt()

void drv_cpu_enableswt(void)
{
// remove the SWT Soft lock
SWT_0.SR.R = 0xC520;
SWT_0.SR.R = 0xD928;
while (SWT_0.CR.B.SLK == 0x1);
/* Enable SWT_0 */
SWT_0.CR.R = 0xFF00010F; // STP = 1, FRZ = 1, WEN = 1
}

3. CPU enter STOP0 mode with _switchMode(STOP0)

void _switchMode(CPUModeTypedef NewMode)
{
MC_ME.MCTL.R = (NewMode<<28)|0x00005AF0; // Enter Mode & Key
MC_ME.MCTL.R = (NewMode<<28)|0x0000A50F; // Enter Mode & Inverted Key
while (MC_ME.GS.B.S_MTRANS) {}; // Wait for mode transition to complete
while(MC_ME.GS.B.S_CURRENT_MODE != NewMode) {}; // Verify NewMode is the current mode
}

4. The CPU will reset after 1 second .

5. If stop SWT then the CPU will keep in STOP0 mode.

Labels (1)
Tags (2)
1 Solution
4,345 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I tested watchdog in STOP mode and it works correct on my side. I created simple example, which demonstrates the functionality of STP bit in  SWT_CR register.

Please see example and also Reset signal. In my example I defined macro STOP_SWT. If this symbol is set to 1, watchdog is stopped in STOP mode, if STOP_SWT is 0, watchdog is running in STOP mode. I tested the example without debugger connected.

First case: SWT is disabled in STOP mode:

1) Reset signal after power on reset

pastedImage_1.jpg

2) Reset signal when microcontroller is running

pastedImage_2.jpg

Second case: SWT is enabled in STOP mode:

1) Reset signal after power on reset

pastedImage_3.jpg

2) Reset signal when microcontroller is running

pastedImage_6.jpg

In the first case you see, there is no reset, because SWT is stopped while microcontroller is in STOP mode (I do not wake up micro from STOP mode in my example).

In the second case there is periodical reset caused by SWT, because SWT is still running, even if microcontroller is in STOP mode.

Please test the example, and let me know if it works on your side.

PS: I did not test your example, but if I were you, I will check the STOP mode at first. Because if there is some pending interrupt or some event, microcontroller does not go to STOP mode and STP bit in SWT has no effect. It is also better to test the example without debugger.

I use MPC5744P 1N15P, so we have the same mask.

Regards,

Martin

View solution in original post

6 Replies
4,345 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

the behavior you describe is correct. If SWT is stopped (microcontroller is not reset after 1 second), microcontroller stays in STOP mode. The normal exit from the STOP0 mode is by an interrupt or a wakeup event (WKPU module, RTC module). Please see reference manual chapter Mode Entry module.

What is your goal? Do you want to switch microcontroller back from stop mode? Please clarify more detail.

Regards,

Martin

0 Kudos
Reply
4,345 Views
hangxie
Contributor III

Hi,

    I want the SWT to stop in STOP0 mode, so I set the STP = 1 in SWT_0.CR, but the CPU always reset after 1 second.

0 Kudos
Reply
4,345 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please share the whole project? I have to check your FCCU settings. Which mask of MPC5744P you use? Do you have your own design or you have NXP EVB?

Regards,

Martin

0 Kudos
Reply
4,345 Views
hangxie
Contributor III

Hi,

   I'm migrating the code from MPC5643L in our own design.  the MPC5744P mask is "1N15P" (samples from Arrow Electronics). 

   The FCCU config is:

   

void _clearFCCUfaults(void)
{
     int32_t i;
     for (i=0;i<3;i++)
     {
          FCCU.NCFK.R = FCCU_NCFK_KEY;
          FCCU.NCF_S[i].R = 0xFFFFFFFF;
          while (FCCU.CTRL.B.OPS != 0x3);
     }
}

void _configFCCU(void)
{
  /* Unlock configuration */
  FCCU.TRANS_LOCK.B.TRANSKEY = 0xBC;

  /* provide Config state key */
  FCCU.CTRLK.R = 0x913756AF;

  /* enter config state - OP1 */
  FCCU.CTRL.R = 0x1;

  /* Verify if state change was sucessful */
  while (FCCU.CTRL.B.OPS != 0x3); //operation status successful

  /* Configure FCCU to react on NCF14 with long functional reset */
  FCCU.NCFS_CFG[0].R = 0x20000000;  //long functional reset reaction

  //set up the NOMAL mode of FCCU
  FCCU.CTRLK.R = 0x825A132B;    //key for OP2
  FCCU.CTRL.R = 0x2;      //set the OP2 - set up FCCU into the NORMAL mode
  while (FCCU.CTRL.B.OPS != 0x3); //operational status succesfull

}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 Kudos
Reply
4,346 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I tested watchdog in STOP mode and it works correct on my side. I created simple example, which demonstrates the functionality of STP bit in  SWT_CR register.

Please see example and also Reset signal. In my example I defined macro STOP_SWT. If this symbol is set to 1, watchdog is stopped in STOP mode, if STOP_SWT is 0, watchdog is running in STOP mode. I tested the example without debugger connected.

First case: SWT is disabled in STOP mode:

1) Reset signal after power on reset

pastedImage_1.jpg

2) Reset signal when microcontroller is running

pastedImage_2.jpg

Second case: SWT is enabled in STOP mode:

1) Reset signal after power on reset

pastedImage_3.jpg

2) Reset signal when microcontroller is running

pastedImage_6.jpg

In the first case you see, there is no reset, because SWT is stopped while microcontroller is in STOP mode (I do not wake up micro from STOP mode in my example).

In the second case there is periodical reset caused by SWT, because SWT is still running, even if microcontroller is in STOP mode.

Please test the example, and let me know if it works on your side.

PS: I did not test your example, but if I were you, I will check the STOP mode at first. Because if there is some pending interrupt or some event, microcontroller does not go to STOP mode and STP bit in SWT has no effect. It is also better to test the example without debugger.

I use MPC5744P 1N15P, so we have the same mask.

Regards,

Martin

4,345 Views
hangxie
Contributor III

Hi,

   I test your example in my board, and it works. So I try to find the different from your code, but there no any different with mine, finally I try to remove the debugger, every works fine! Great Thanks!!