MPC5744P SRAM ECC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5744P SRAM ECC

跳至解决方案
3,071 次查看
Danielyuyu
Contributor I

Recently, I have been trying to change the SRAM of MPC5744P and have found some issues. I hope someone can help me solve them. The problem is that after completing initialization, I receive messages through the CAN bus in a dead loop and change the data of the SRAM when the message is valid and triggered. The code for changing SRAM is as follows:

uint8_t i;
for(i=0;i<32;i++)
{
*(uint8_t *)(0x40000000+i) = 0xFF;
}

When I changed the SRAM at the above address(0x40000000), MPC5744P experienced a reset, and I believe it triggered the SRAM ECC. Of course, the SRAM part I modified was not used by the system. I cleared the 1KB area of SRAM starting from 0x4000000 by modifying the connection file. Code below:

/* Entry Point */
ENTRY(_start)

/* define heap and stack size */
__HEAP_SIZE = 0 ;
__STACK_SIZE = 4096 ;

SRAM_SIZE = 383K;
/* Define SRAM Base Address */
SRAM_BASE_ADDR = 0x40000000;

/* Define CPU0 Local Data SRAM Allocation */
LOCALDMEM_SIZE = 64K;
/* Define CPU0 Local Data SRAM Base Address */
LOCALDMEM_BASE_ADDR = 0x50800000;

MEMORY
{
flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0004, len = 0x4

reboot_start_check : org = 0x00FA0100, len = 0x10
m_text : org = 0x00FA0400, len = 190K
reboot_end_check : org = 0x00FCFC00, len = 0x10

m_data : org = 0x40000400, len = 383K

local_dmem : org = 0x50800000, len = 64K
}

Although I have freed up some SRAM, it will still reset after modifying the data for that address. So I turned off the SRAM ECC initialization in the startup file and found that the reset phenomenon disappeared. Here is the code I blocked:

;#***************************** Initialise SRAM ECC ***************************/
;# Store number of 128Byte (32GPRs) segments in Counter
e_lis r5, __SRAM_SIZE@h # Initialize r5 to size of SRAM (Bytes)
e_or2i r5, __SRAM_SIZE@l
e_srwi r5, r5, 0x7 # Divide SRAM size by 128
mtctr r5 # Move to counter for use with "bdnz"

;# Base Address of the internal SRAM
e_lis r5, __SRAM_BASE_ADDR@h
e_or2i r5, __SRAM_BASE_ADDR@l

;# Fill SRAM with writes of 32GPRs
sram_loop:
e_stmw r0,0(r5) # Write all 32 registers to SRAM
e_addi r5,r5,128 # Increment the RAM pointer to next 128bytes
e_bdnz sram_loop # Loop for all of SRAM

My question is why writing SRAM through addresses and pointers triggers ECC, or other issues are causing my situation to occur. What if I want to enable ECC for SRAM and manually modify SRAM?

 

0 项奖励
回复
1 解答
3,016 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I see no issue here in storing anything in RAM.

The point is the ECC is HW implementation on the RAM array. So any write will create valid data+valid ECC syndrome.

The issue is when you try to read RAM where the ECC is not initialized. For example after destructive reset when in RAM are random data and do not match the ECC syndrome.

So either first initialize ECC in RAM or do not use read operations (like read modify write) before you initialize the ECC. Writes are fine and will simply initialize the ECC.

I see no issue in your approach, simply make sure your ECC in RAM is initialized before you read RAM.

Best regards,

Peter

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,042 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The ECC is always enabled on this device.

So you have to do initialization before you use the RAM. If not, then on the first read you will get exception because of multibit ECC faults.

Next, you can read your reset reason in FCCU NCFSx registers and in RGM FES and DES registers.

Right after reset you will have logged fault there. so It is good to set some break points at start of code to prevent overwrite of these status registers.

Have a look at FCCU and RGM chapters in reference manual.

Best regards,

Peter

0 项奖励
回复
3,026 次查看
Danielyuyu
Contributor I

Dear Peter,

Thank you very much for your reply!

I am developing a flash driver for automotive ECU which cannot be fixed in Flash. When there is a usage requirement, the upper computer issues the flash driver package, and I need to store it in RAM. If there is ECC detection, how can I temporarily store the code in RAM?

0 项奖励
回复
3,017 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I see no issue here in storing anything in RAM.

The point is the ECC is HW implementation on the RAM array. So any write will create valid data+valid ECC syndrome.

The issue is when you try to read RAM where the ECC is not initialized. For example after destructive reset when in RAM are random data and do not match the ECC syndrome.

So either first initialize ECC in RAM or do not use read operations (like read modify write) before you initialize the ECC. Writes are fine and will simply initialize the ECC.

I see no issue in your approach, simply make sure your ECC in RAM is initialized before you read RAM.

Best regards,

Peter

0 项奖励
回复
3,010 次查看
Danielyuyu
Contributor I
thanks a lot! Peter
wish u have a good day
0 项奖励
回复