MPC5744P SPI TX problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P SPI TX problem

Jump to solution
2,169 Views
mark_registraci
Contributor II

Hello,

I want to send some data (0xF0F0) with SPI on MPC5744P, but there is no activity on any of the signals (CLK, CS, MISO or MOSI). Am I doing something wrong? If I understand correctly, after write to PUSHR there should be something in the TXFR registers, but there isn't.

void SysClk_Init(void)
{
MC_CGM.AC3_SC.R = 0x01000000; //Connect XOSC to the PLL0 input.
MC_CGM.AC4_SC.R = 0x03000000; //Connect PLL0_PHI1 to the PLL1 input.

//Set PLL0 to 160 MHz with 40 MHz XOSC reference.
PLLDIG.PLL0DV.R = 0x40024020; //PREDIV = 4, MFD = 32, RFDPHI = 2, RFDPHI1 = 8

MC_ME.RUN0_MC.R = 0x00130070; // RUN0 cfg: IRCON,XOSCON,PLL0ON,syclk=IRC

// Mode Transition to enter RUN0 mode:
MC_ME.MCTL.R = 0x40005AF0; // Enter RUN0 Mode & Key
MC_ME.MCTL.R = 0x4000A50F; // Enter RUN0 Mode & Inverted Key
while (MC_ME.GS.B.S_MTRANS) {}; // Wait for mode transition to complete
while(MC_ME.GS.B.S_CURRENT_MODE != 4) {}; // Verify RUN0 is the current mode

//Set PLL1 to 200 MHz with 40 MHz PLL0_PHI1 input.
PLLDIG.PLL1DV.R = 0x00020014; //MFD = 20, RFDPHI = 2
PLLDIG.PLL1FD.R = 0x00000000; //EnableandconfigurationfractionalmultiplierforPLL1

MC_ME.RUN_PC[0].R = 0x000000FE; //Enable peripherals to run in all modes
MC_ME.RUN0_MC.R = 0x001300F4; // RUN0 cfg: IRCON, XOSCON, PLL0ON, PLL1ON, syclk=PLL1_PHI

MC_CGM.SC_DC0.R = 0x80030000; //Divide system clock by 4 to achieve PBRIDGEx_CLK of 50 MHz

// Mode Transition to enter RUN0 mode:
MC_ME.MCTL.R = 0x40005AF0; // Enter RUN0 Mode & Key
MC_ME.MCTL.R = 0x4000A50F; // Enter RUN0 Mode & Inverted Key
while (MC_ME.GS.B.S_MTRANS) {}; // Wait for mode transition to complete
while(MC_ME.GS.B.S_CURRENT_MODE != 4) {}; // Verify RUN0 is the current mode
}

void InitPeriClkGen(void)
{
MC_CGM.SC_DC0.R = 0x80030000; //PBRIDGEx_CLK at system clock divided by 4 (50 MHz).
MC_CGM.AC0_SC.R = 0x02000000; //Select PLL0_PHI as source of Auxiliary Clock 0.
MC_CGM.AC0_DC0.R = 0x80000000; //MOTC_CLK: Enabled at Auxiliary Clock 0 divide by 1(160 MHz).
MC_CGM.AC0_DC1.R = 0x80070000; //SGEN_CLK: Enabled at Auxiliary Clock 0 divide by 8(20 MHz).
MC_CGM.AC0_DC2.R = 0x80010000; //ADC_CLK: Enabled at Auxiliary Clock 0 divide by 2(80 MHz).

/* Auxiliary Clock 1 is always sourced from PLL0_PHI. */
MC_CGM.AC1_DC0.R = 0x80010000; //FRAY_CLK: Enabled at Auxiliary Clock 1 divided by 2 (40 MHz).
MC_CGM.AC1_DC1.R = 0x80010000; //SENT_CLK: Enabled at Auxiliary Clock 1 divided by 2 (80 MHz).

/* Auxiliary Clock 2 is always sourced from PLL0_PHI. */
MC_CGM.AC2_DC0.R = 0x80010000; //CAN_CLK: Enabled at Auxiliary Clock 2 divided by 2 (40 MHz).

MC_CGM.AC5_SC.R = 0x02000000; //Select PLL0_PHI as source of Auxiliary Clock 5.
MC_CGM.AC5_DC0.R = 0x80070000; //LFAST_PLL: Enabled at Auxiliary Clock 5 divided by 8 (20 MHz).

MC_CGM.AC6_SC.R = 0x04000000; //Select PLL1_PHI as source of Auxiliary Clock 6.
MC_CGM.AC6_DC0.R = 0x80000000; //CLKOUT0: Enabled at Auxiliary Clock 6 divided by 1 (200 MHz).

MC_CGM.AC10_SC.R = 0x04000000; //Select PLL1_PHI as source of Auxiliary Clock 10.
MC_CGM.AC10_DC0.R = 0x80030000; //ENET_CLK: Enabled at Auxiliary Clock 10 divided by 4 (50 MHz).

MC_CGM.AC11_SC.R = 0x04000000; //Select PLL1_PHI as source of Auxiliary Clock 11.
MC_CGM.AC11_DC0.R = 0x80030000; //ENET_TIME_CLK: Enabled at Auxiliary Clock 10 divided by 4 (50 MHz).

/* DSPI 0 */
MC_ME.PCTL99.B.RUN_CFG = 0x0;
}

void SPI()

{

// chip select
SIUL2.MSCR[MSCR_SPI_CS].B.SSS = 1;
SIUL2.MSCR[MSCR_SPI_CS].B.OBE = 1;
SIUL2.MSCR[MSCR_SPI_CS].B.SRC = 3;
// clock
SIUL2.MSCR[MSCR_SPI_CLK].B.SSS = 1;
SIUL2.MSCR[MSCR_SPI_CLK].B.OBE = 1;
SIUL2.MSCR[MSCR_SPI_CLK].B.SRC = 3;
// MOSI
SIUL2.MSCR[MSCR_SPI_MOSI].B.SSS = 1;
SIUL2.MSCR[MSCR_SPI_MOSI].B.OBE = 1;
SIUL2.MSCR[MSCR_SPI_MOSI].B.SRC = 3;
// MISO
SIUL2.MSCR[MSCR_SPI_MISO].B.IBE = 1;
SIUL2.IMCR[IMCR_SPI_MISO].B.SSS = 1;

SPI_0.MCR.B.MSTR = 1;
SPI_0.MCR.B.DCONF = 0x0;
SPI_0.MCR.B.FRZ = 0;
SPI_0.MCR.B.PCSIS = 0x01;
SPI_0.MCR.B.HALT = 1;

SPI_0.MODE.CTAR[0].B.DBR = 0;
SPI_0.MODE.CTAR[0].B.FMSZ = 0xF;
SPI_0.MODE.CTAR[0].B.CPOL = 0;
SPI_0.MODE.CTAR[0].B.CPHA = 0;
SPI_0.MODE.CTAR[0].B.LSBFE = 0; // MSB first
SPI_0.MODE.CTAR[0].B.PBR = 0;
SPI_0.MCR.B.HALT = 0; // start module

SPI_0.PUSHR.PUSHR.R = 0x0801F0F0; // EOQ=1, PCS=1, TXDATA=0xF0F0

uint16_t tx_command = SPI_0.TXFR[4].B.TXCMD_TXDATA;
uint16_t tx_data = SPI_0.TXFR[4].B.TXDATA;

}

0 Kudos
Reply
1 Solution
1,958 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the code looks normal. It is not clear which pins is configured, also you set quite high baudrate. 

If placing single word to TXFIFO, TXFR[0] can be checked.

Attached you have simple code for SPI0 transmit.

Hope it helps.

BR, Petr

View solution in original post

0 Kudos
Reply
1 Reply
1,959 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the code looks normal. It is not clear which pins is configured, also you set quite high baudrate. 

If placing single word to TXFIFO, TXFR[0] can be checked.

Attached you have simple code for SPI0 transmit.

Hope it helps.

BR, Petr

0 Kudos
Reply