MPC5744P Reasign INTC Interrupt Handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P Reasign INTC Interrupt Handler

ソリューションへジャンプ
3,973件の閲覧回数
moaheux
Contributor I

Hi,

I'm struggling with the INTCinterrupt handler. I did create a bootloader and scheduled a function to be called every 1ms using 

INTC_InstallINTCInterruptHandler(PIT_ISR0, (uint8_t) (PIT_INTERRUPT_VECTOR_CH0), (uint8_t) priority);
 
void PIT_ISR0() {
    dummy();   
    PIT_0.TIMER[0].TFLG.R = 1;
}
Everything is working fine till I jump to the application and it appear that I can't update a vector previously set with a new Function.
 
Would you have any tips how to de-initialize the INTC properly ?

Thanks in advance.
0 件の賞賛
返信
1 解決策
3,954件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the most important thing is to disable all interrupts on all levels before jump to an application: by MSR[EE] bit, by local enable bits in peripherals, by priorities in INTC. This is usually the reason for most of the troubles. It's also good idea to de-initialize all used peripherals to default reset state.

Regards,

Lukas

元の投稿で解決策を見る

2 返答(返信)
3,937件の閲覧回数
moaheux
Contributor I

Hi lukaszadrapa,

You found exactly the good point I missed the MSR[EE] bit. It' now working like a charm. Thanks a lot, I wasted so much time on it.

I'll attach my sample code to this thread so people with the same problem will have the chance to go through.

0 件の賞賛
返信
3,955件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the most important thing is to disable all interrupts on all levels before jump to an application: by MSR[EE] bit, by local enable bits in peripherals, by priorities in INTC. This is usually the reason for most of the troubles. It's also good idea to de-initialize all used peripherals to default reset state.

Regards,

Lukas