MPC5744P PWM capture problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P PWM capture problem

1,345 Views
eric_lau
Contributor I

Hi,sir:

    

I am a new to use  the function of FlexPWM capture about  MPC5744p. In  the process of using, I had a promblem.

      I use the PIN of X2 (G[2]) as the input port to capture the signal , used FlexPWM capture rigester,used Uart receive the value of Pulse width. What i recerved on the uart,Pulse width  is 78.However,the signal  is 100hz ,50% duty. Is my result right? Who can tell me how to confiure the rigester ,how to measure the period and the pulse width?

 Blow are my init code and ISR code.

void SUIL2_PWMIN_Init(void)
{
SIUL2.MSCR[PC11].R = 0x32000000; //PC[11] GPIO - Red LED
SIUL2.MSCR[PC12].R = 0x32000000; //PC[11] GPIO - Red LED
SIUL2.GPDO[PC12].R = 1;
SIUL2.GPDO[PC11].R = 1;

SIUL2.MSCR[PG2].B.SRC = 3; /* Pad: Maximum slew rate */
SIUL2.MSCR[PG2].B.SMC = 1; /* Pad: Safe Mode Control Enable */
SIUL2.MSCR[PG2].B.HYS = 1; /* Pad: Input Hysteresis Enable */
SIUL2.MSCR[PG2].B.PUS = 1; /* Pad: PullUP */
SIUL2.MSCR[PG2].B.PUE = 1; /* Pad: Pull Enable */
SIUL2.MSCR[PG2].B.IBE = 1; /* Pad: Enable pad for input */
SIUL2.IMCR[96].B.SSS = 2; /* connected to pad flexpwm0 X2 */

SIUL2.MSCR[PG5].B.SRC = 3; /* Pad: Maximum slew rate */
SIUL2.MSCR[PG5].B.SMC = 1; /* Pad: Safe Mode Control Enable */
SIUL2.MSCR[PG5].B.HYS = 1; /* Pad: Input Hysteresis Enable */
SIUL2.MSCR[PG5].B.PUS = 1; /* Pad: PullUP */
SIUL2.MSCR[PG5].B.PUE = 1; /* Pad: Pull Enable */
SIUL2.MSCR[PG5].B.IBE = 1; /* Pad: Enable pad for input */
SIUL2.IMCR[99].B.SSS = 3; /* connected to pad flexpwm0 X3 */
}

void FlexPWM_IN_Init()
{
FlexPWM_0.SUB[2].CTRL1.R = 0x0474; // full cycle reload, PWM 128 clock frequency = fclk/128=1.25mhz,fclk=160MHZ
FlexPWM_0.SUB[2].DTCNT0.R = 0x0000; 
FlexPWM_0.SUB[2].DTCNT1.R = 0x0000; 
FlexPWM_0.SUB[2].INIT.R = 0; // PWM  init count value
FlexPWM_0.SUB[2].VAL0.R = 6250;
FlexPWM_0.SUB[2].VAL1.R = 12500; //100HZ val1=(1/freq)*(fclk/128) period
FlexPWM_0.SUB[2].DISMAP.R = 0x0000; // disable fault pin condition

FlexPWM_0.MCTRL.B.LDOK = 0x0f; //PWM module 0,1,2,3 load init value.


FlexPWM_0.SUB[2].INTEN.B.CX0IE= 1; // CIE0 enable interrupt
FlexPWM_0.SUB[2].INTEN.B.CX1IE= 1; // CIE1 enable interrupt

FlexPWM_0.SUB[2].CAPTCTRLX.B.EDGX0= 2; // CAPT0  capture rising edge
FlexPWM_0.SUB[2].CAPTCTRLX.B.EDGX1= 1; // CAPT1  capture falling edge
FlexPWM_0.SUB[2].CAPTCTRLX.B.ONESHOTX= 1; // one shot mode


}

*******************************************************************************/
void FlexPWM_CAF2_ISR(void)
{

if(FlexPWM_0.SUB[2].STS.B.CFX0)//CAP0 interrupt
{
rising_edge= FlexPWM_0.SUB[2].CVAL0.R; // read cap0 rising edge
num1 = FlexPWM_0.SUB[2].CVAL0CYC.R;//

falling_edge= FlexPWM_0.SUB[2].CVAL1.R; //  read cap1 falling edge
num2 = FlexPWM_0.SUB[2].CVAL1CYC.R;//
SIUL2.GPDO[PC12].R = 0;//
}
FlexPWM_0.SUB[2].STS.R = 0x00C0; // clear CFX1/CFX0  flag
Pulse_width =falling_edge-rising_edge;
Duty=(UInt32)Pulse_width*100/Period;
capture_over=1;
}

Thank you can  provide source code and some information.

Thank you  very much for you hlep.

Labels (1)
0 Kudos
Reply
0 Replies