MPC5744P DCF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,394件の閲覧回数
Du_0224
Contributor III
Respected NXP engineer: Hello, I am using MPC5744P, and I want to ask a question about DCF Records. I mistakenly write all the data in part of the address (0x00400200-0x00400300) of DCF Records as 00. This caused me to be unable to debug via JTAG (PEmicro). Is there any way to save it.
タグ(2)
0 件の賞賛
返信
1 解決策
3,384件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Unfortunately not. This is just the situation leading in permanent lock of the device.

UTEST area (where DCF records are being stored) is OTP area (one time programmable), once you program it you cannot erase it.

I am sorry for bad news.

元の投稿で解決策を見る

3 返答(返信)
3,385件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Unfortunately not. This is just the situation leading in permanent lock of the device.

UTEST area (where DCF records are being stored) is OTP area (one time programmable), once you program it you cannot erase it.

I am sorry for bad news.

1,965件の閲覧回数
FKS
Contributor II

      Hello, I have a question. I found in the MPC5744P Reference Manual that there is a description about the factory erase mechanism. Does this mean that if I forget the password, I can use this mechanism to unlock it? If so, could you please provide some examples or notes to show me how to use the factory erase mechanism?

     Thank you very much. I am eagerly looking forward to your reply.FKS_0-1748425010912.png

 

 

タグ(1)
0 件の賞賛
返信
1,946件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

This feature is not available for users, it can only be erased in NXP factory.

0 件の賞賛
返信